mcuxpressoide_packages_support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcuxpressoide_packages_support

ソリューションへジャンプ
2,658件の閲覧回数
cavinlong
Contributor I

Hi, 

Can I know what the purpose of the mcuxpressoidle_packages_support files is?

I know it was an auto-generated workspace files, but can we actually delete it?

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,624件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @cavinlong,

These files cannot be deleted, as they are needed for the proper integration of the installed SDKs with MCUXpresso. If modified or deleted, the IDE will automatically regenerate these files on SDK refresh.

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,092件の閲覧回数
VassiliN
Contributor III

I have a related question. Maybe there is some information about SDK version/git/MCUXpresso in the community, I would appreciate if you can show me the right direction. 

 

Now the issue I have at hand. 

I just put my source code of the applications being developed with MCUXpresso under the git control. Applications use SDK version (say) 2.15. 

 

.metadata/ line was added by the MCUXpresso automatically to .gitignore. Fine. 

 

Now I installed MCUXpresso on the second computer, but the SDK 2.15 is not available on NXP anymore. So installed SDK 2.16 instead. 

Now when I pull the source code from the git, it overwrites the content of .mcuxpressoide_packages_support/ on the second computer. 

When I start MCUXpresso on the second machine,  .mcuxpressoide_packages_support/ is overwritten again. 

I assume I can put .mcuxpressoide_packages_support/ in .gitignore, since each project includes the copies of all the files from SDK anyways. Then I have to be careful if a need to add something from the SDK, I should do it only on the computer where I have original version of the SDK, right? 

 

However, my question is what is the recommended way to keep the SDK versions synchronized, using git and MCUXpresso?

How I install the previous version of SDK 2.15 on the second machine and force MCUXpresso to use it instead of the later 2.16?

How I migrate my code in git to the next version of SDK when I need it?  

0 件の賞賛
返信
2,625件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @cavinlong,

These files cannot be deleted, as they are needed for the proper integration of the installed SDKs with MCUXpresso. If modified or deleted, the IDE will automatically regenerate these files on SDK refresh.

BR,
Edwin.

0 件の賞賛
返信