lwIP for LPC4350

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lwIP for LPC4350

1,592件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Wed Jan 25 16:04:51 MST 2012
Are there any plans to add support for the LPC4350 in the lwIP library?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,569件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Fri Jan 27 08:36:02 MST 2012
I just put a FreeRTOS 7.1.0 port for the LPC4350 on the www.FreeRTOS.org website.  This application runs on the Hitex LPC4350 Eval board.  You can go to the FreeRTOS interactive section, select community contributions, select the contributed files link and click on NXP to obtain the code.  Hope this helps with the lwIP port.  If you get any preliminary version completed, I would love to help you test it.

Thanks
Greg Dunn
[email protected]
0 件の賞賛
返信

1,569件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Wed Jan 25 17:15:09 MST 2012
Yes - a port for the LPC18xx and LPC43xx will be available soon using the on-chip MAC. Like the 17xx port, it will support standalone operation, zero-copy transfers and support for GNU, Keil, and IAR toolchains. This one will (probably) also be pre-integrated with FreeRTOS and have some extra features over the basic 17xx port. Unofficially, I'd say around late February or early March for this.
0 件の賞賛
返信