lpcxpresso54628 beginning issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpcxpresso54628 beginning issue.

ソリューションへジャンプ
3,962件の閲覧回数
saideva293
Contributor II

Hi,

Im new to this MCU,i bought the lpcxpresso54628 and made the initialization using  given guides from the nxp website.

I did my first example program in the dev board. but, unfortunately the GUI which appeared in LCD display before initialization is not appearing after flashing an example program.I want to know is that a problem or not and why it happened,guide me.

ラベル(1)
1 解決策
3,847件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The LPCXpresso54628 out of factory board is programmed emWin demo inside.

Your demo code should not support LCD display, and it overwrite the original demo.

If you want it, you can get the emWin demo from here:

OM13098 | LPCXpresso Development Board | LPC Microcontrollers (MCUs) | NXP 

Binaries for rolling demo of emWIN features on LPCXpresso54608

Please note, this package includes only burning code.  the source code is not published.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
3,847件の閲覧回数
saideva293
Contributor II

thank you!

0 件の賞賛
返信
3,847件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

welcome!

0 件の賞賛
返信
3,848件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The LPCXpresso54628 out of factory board is programmed emWin demo inside.

Your demo code should not support LCD display, and it overwrite the original demo.

If you want it, you can get the emWin demo from here:

OM13098 | LPCXpresso Development Board | LPC Microcontrollers (MCUs) | NXP 

Binaries for rolling demo of emWIN features on LPCXpresso54608

Please note, this package includes only burning code.  the source code is not published.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,847件の閲覧回数
converse
Senior Contributor V

The program running on the device when shipped, will be overwritten when you program your own application onto the device. So, this is not a problem.

3,847件の閲覧回数
saideva293
Contributor II

Thank you!

How can i get back the previous one is that possible?

0 件の賞賛
返信