lpc832 PWM on multiple pins simultaneously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc832 PWM on multiple pins simultaneously

ソリューションへジャンプ
2,280件の閲覧回数
aaronm
Contributor IV

Hi, I'm working with an LPC832 by itself on a custom board - it's not an evaluation kit; SDK version 2.13.0 from 1/18/23 - and I can't get more than one PWM signal to work at a time.  The one pin that does work works fine and as expected, but the two other pins I want to run PWM on don't send a signal: I'm using an oscilloscope to watch for them on the output pins.  All three are configured the same way.

I see in the Pins page, Peripherals panel the following section - see image - and now I'm wondering if only one PWM signal is allowed at a time.  Is that what is meant by "routable to 16 pins, 1 signal" in the attached image?  If not, how do I get more than one PWM signal simultaneously?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
aaronm
Contributor IV

Never mind.  I figured it out: I had too many "states" defined - bottom of the SCT peripheral configuration page - and those conditions were never reached.  I removed states "1" and "2" and combined all PWM Signals in state 0.  It now works as expected.  I'll be the first to admit I'm just poking around, here, and don't really know what I'm doing.  But at least it's now working.

Screenshot 2023-03-08 at 1.28.49 AM.pngScreenshot 2023-03-08 at 1.28.49 AM.png

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,268件の閲覧回数
aaronm
Contributor IV

Never mind.  I figured it out: I had too many "states" defined - bottom of the SCT peripheral configuration page - and those conditions were never reached.  I removed states "1" and "2" and combined all PWM Signals in state 0.  It now works as expected.  I'll be the first to admit I'm just poking around, here, and don't really know what I'm doing.  But at least it's now working.

Screenshot 2023-03-08 at 1.28.49 AM.pngScreenshot 2023-03-08 at 1.28.49 AM.png

0 件の賞賛
返信