lpc824 with lpcopen using uart and dma receive variable length data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc824 with lpcopen using uart and dma receive variable length data

1,550 Views
chengguozhang
Contributor I

Can somebody help me to achieve receiving the data which length is variable via uart (perhaps with dma?),thanks a lot

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,349 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Chengguo, 

The LPC824 apart of the LPCOpen has a code bundle. The code bundle does have a example of UART with DMA, also another good point of the code bundle is that the examples doesn't add so much overhead as the ones of the LPCOpen. 

If you are working with MCUXpresso IDE you will find the code bundle in the next path:

C:\nxp\MCUXpressoIDE_10.1.1_606\ide\Examples\CodeBundles

In LPCXpresso the path is the following:

C:\nxp\LPCXpresso_8.2.2_650\lpcxpresso\Examples\CodeBundles

Hope it helps!

Victor.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply