lpc824 with lpcopen using uart and dma receive variable length data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc824 with lpcopen using uart and dma receive variable length data

1,554件の閲覧回数
chengguozhang
Contributor I

Can somebody help me to achieve receiving the data which length is variable via uart (perhaps with dma?),thanks a lot

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,353件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Chengguo, 

The LPC824 apart of the LPCOpen has a code bundle. The code bundle does have a example of UART with DMA, also another good point of the code bundle is that the examples doesn't add so much overhead as the ones of the LPCOpen. 

If you are working with MCUXpresso IDE you will find the code bundle in the next path:

C:\nxp\MCUXpressoIDE_10.1.1_606\ide\Examples\CodeBundles

In LPCXpresso the path is the following:

C:\nxp\LPCXpresso_8.2.2_650\lpcxpresso\Examples\CodeBundles

Hope it helps!

Victor.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信