lpc54s018-lpc5418 jump from custom boot to firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc54s018-lpc5418 jump from custom boot to firmware

3,742 次查看
ppardo
Contributor II

Hi,

We currently use a pc54s018j2m.

During development, our main firmware is located at default "program_flash" address 0x10000000 and it works fine.

During production, we create another firmware (a monitor) that become our boot firmware (also located at "program_flash" address 0x10000000).

We change "program_flash" address for the main firmware to be 0x10060000, and program the flash with generated code.

We now want to jump to this address from the monitor.

Here's my jump procedure:

__RAMFUNC(RAM2) void execute_code(unsigned addr)
{
   __ISB();
   __DSB();

   __ASM volatile ("cpsid i");
   __ASM volatile ("cpsid f");

   SCB->VTOR = addr;
   uint32_t *p;
   p = (uint32_t*) addr;
   __set_MSP(*p);
   __set_PSP(*p);

   p++;
   void (*user_code_entry)(void) = NULL;
   user_code_entry = (void (*)(void)) (*p);
   user_code_entry();
}

 

And I call this function with following code:

execute_code(0x10060000);

 

And.. it crashes.

 

Is there any problem with my execute_code function (this functions works fine on lpc55s28, but maybe it's completely different).

 

Do you have any hints ? or link ?

 

regards

 

标签 (1)
标记 (1)
0 项奖励
回复
11 回复数

3,583 次查看
ppardo
Contributor II

@xiangjun_rong @Alice_Yang 

Is it possible to have a simple reply ?

On my lpc54s018

* I've a 1st firmware (called Boot) at address 0x10000000 (defined in IDE MCU settings)

* I've a 2nd firmware (called Firmware) at address 0x10060000 (defined in IDE MCU settings)

Both are programmed with segger jflash (data file, merge data file), and memory is checked.

Now how can I jump from my first Boot to my Firmware.

 

I explain in a previous post how I try to do this jump, but it don't work and any advice will be welcome.

I follow many application notes, check many example but don't find anything.

Is it possible ? And how ?

 

Regards

 

0 项奖励
回复

3,691 次查看
frank_m
Senior Contributor III

Not sure if this is relevant here ...
But wouldn't you need to have an "odd" target address as jump location ?
The LSB of the address serves as marker for the core mode in several instructions, with "0" meaning ARM mode, and "1" being Thumb mode.
Instructions are always word-aligned, so ARM reused the LSB here.

0 项奖励
回复

3,728 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the LPC55S69, there is an example hello_world for trustzone, in the application, there is a part of code to do the almost same job, I copy it here.

typedef void (*funcptr_ns)(void) TZM_IS_NONSECURE_CALLED;

 

void TZM_JumpToNormalWorld(uint32_t nonsecVtorAddress)
{
funcptr_ns ResetHandler_ns;

/* Set non-secure main stack (MSP_NS) */
__TZ_set_MSP_NS(*((uint32_t *)(nonsecVtorAddress)));

/* Set non-secure vector table */
SCB_NS->VTOR = nonsecVtorAddress;

/* Get non-secure reset handler */
ResetHandler_ns = (funcptr_ns)(*((uint32_t *)((nonsecVtorAddress) + 4U)));

/* Call non-secure application - jump to normal world */
ResetHandler_ns();
}

#define DEMO_CODE_START_NS 0x00010000

#define NON_SECURE_START DEMO_CODE_START_NS

 

TZM_JumpToNormalWorld(NON_SECURE_START);

 

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复

3,722 次查看
ppardo
Contributor II
Thanks for the reply,

I'll try your advice asap, but

in my case, i'm not in a trusted zone. My monitor is just un simple app in extern flash that needs to jump to another app (in external flash).


regards,

pierre
0 项奖励
回复

3,700 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pierre,

Yes, I see that you do not use trustzone. But the scenario is the same, pls refer to it.

BR

XiangJun Rong

 

0 项奖励
回复

3,696 次查看
ppardo
Contributor II

Hi,

thank your for reply.

But what kind of address do I have to use.

 

My bootloader is in external flash (addresse 0x10000000)

My firmware is in external flash (address 0x10060000)

 

Do I have to try a jump to address 0x10060000 or to address 0x60000 ?

Is there special advice about spifi configuration ?

Is there special advice about timers, reset, ...

 

Regards

pierre

0 项奖励
回复

3,680 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For LPC540xx family, the SPIFI address space is from ox1000_0000 to 0x17FF_FFFF, so jumping  to address 0x10060000 is correct.

Pls refer to the an12384.pdf, which can be downloaded from the web site:

https://www.nxp.com.cn/docs/en/application-note/AN12384.pdf

This is the jumping code from bootloader to application:

xiangjun_rong_0-1675840126350.png

pls refer to the code

Hope it can help you

BR

XiangJun Rong

3,635 次查看
ppardo
Contributor II

@xiangjun_rongDo you have any advice about my last post ?

We're completely stuck now ?

Is there any sample of a secondary bootloader on lpc54s18, with a jump to external flash (0x10000000 and more) ?

 

Regards

pierre

0 项奖励
回复

3,674 次查看
ppardo
Contributor II

Hi,

Still not work, event by following what's inside AN12384. But I can give you more information about my tests. I reduce all to juste relevant part to have a minimal example of what's not working.

 

I've got 2 simple programs.

* TestBoot (MCU settings: PROGRAM_FLASH 0x10000000, SIZE 0x60000)

  - Plain Load Image SRAMX

  - Global Data Placement SRAM_0_1_2_3

* TestFirmware (MCU settings: PROGRAM_FLASH 0x10060000, SIZE 0x60000)

- Plain Load Image SRAMX

- Global Data Placement SRAM_0_1_2_3

 

Both are very simple:

* TestBoot configure some gpio and blink led.

* Then jump to TestFirmware (0x10060000)

* TestFirmware configure some gpio and blink led (other color)

 

I program both in my external flash with jflash (with data and merge data):

* TestBoot at 0x10000000

* TestFirmware at 0x10060000

I reset the device:

* I see expected led from TestBoot blink

* When the jump occurs, there's a reset on the device, and I fall back to the TestBoot blink

* And so on

I never saw the led from TestFirmware.

I try different code in firmware (with or without GPIO configuration), but I do think that the problem is the jump code that cannot reach my TestFirmware application.

 

Here's the jump function:

static void boot_tofwimage(unsigned addr) // depuis l'AN12384
{
void (*firmwareFunc)(void);
uint32_t fwStack = *((uint32_t*) (addr));
uint32_t fwEntry = *((uint32_t*) (addr + 4U));

firmwareFunc = (void (*)(void)) fwEntry;

SCB->VTOR = addr;
__set_MSP(fwStack);
__set_PSP(fwStack);

firmwareFunc();// let's go
}

 

What's seems weird to me: If I run my TestBoot app step by step, and the firmwareFunc() jumps to ResetISR() that restart the TestBoot !

 

The main difference between the LPC54s18 and the one in AN (LPC5460) is the fact that there's no flash inside.

So, do you have an AN that I can read for a device like the LPC54s18.

Do I have to ensure special features when I compile my firmware ? Options, relocation ?

Do I have to transfer something in RAM ? ...

 

 

My project is completely stuck without a valid bootloader, so any advice will be welcome.

I can perform some tests if needed.

 

Regards

0 项奖励
回复

3,590 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Maybe the spifi interface is not initialized or whatever.

Pls refer to an12352

https://www.nxp.com.cn/docs/en/nxp/application-notes/AN12352.pdf

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

3,677 次查看
ppardo
Contributor II

Thank you,

seems similar to my code, but I'll readd whole doc and follow your advices.

Regards

 

0 项奖励
回复