lpc5460x cannot work after power up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc5460x cannot work after power up

2,995件の閲覧回数
yanqinghe
Contributor I

Dear NXP:

     My chip is lpc54608s512 ,  it's a strange phenomenon ; The MCU works normal for a lot of days, but one day, it can't works after power up , and need power up twice then it works well too;  If the two power up interval too long ,it's can't  works too;

      Do you know what's the matter with the MCU?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,542件の閲覧回数
jw145
Contributor I

We have a similar issue as well, very confused why it is happening. Happens the same on 3/3 custom PCBs but not every time we power them on. 

0 件の賞賛
返信

2,786件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi yanqinghe,

Are you using an evaluation board? Does the same happen if you are running a simple demo program?

You mention that if the interval between the two resets is long then it can work, right? This sounds like a capacitor in your board is still charged and the remaining voltage is preventing the MCU from powering up correctly.

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,786件の閲覧回数
yanqinghe
Contributor I

Dear Carlos Mendoza:

        I'm not using an evaluation board, we designed the board refer to the evaluation board.

I means if the interval between the two resets is long then it can't work; It looks like a capacitor must charge and then the MCU can power up ;  Another phenomenon is when the MCU can't power up , the system 3.3V was pull down to 1.6V, the MCU temperature is a little high. After power off and power up the board at once, the board works normal, the software running well too ; when the MCU is running  it looks well and the temperature is right too;

  

Best Regards

  Yan

0 件の賞賛
返信

2,786件の閲覧回数
nikolastojkov
Contributor I

Dear Yan,

We are experiencing the same issue on our boards. Did you fiund out the root cause of the issue ?

BR

Nikola

0 件の賞賛
返信