lpc4337 USB connect to multiple devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc4337 USB connect to multiple devices

1,051 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhall0819 on Thu Feb 06 09:50:41 MST 2014
Hi,
I am using the LPC4337 in a USB application that needs to connect via USB0 (host) port to 4 downstream devices. My board has a Cypress CY7C65632 hub controller connected to USB0. I have used LPCopen examples for a single device connected to USB1 - works fine. questions:

1. Does the N_PORTS field (fixed at 1) in the HCSPARAMS register indicate the USB controller only supports 1 down stream device.

2. If so is there a software workaround to support multiple device.

3. Can anybody recommend another library or application note that would show how to support multiple devices

Thanks

Labels (1)
0 Kudos
Reply
0 Replies