lpc4330 static memory configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc4330 static memory configuration

1,610 Views
cyc583723081
Contributor I

How to configure an external static memory controller for lpc4330?I tried to write it, but I didn't succeed.The following is my configuration code,please advise

void Board_ExSram_Init(void)
{
IP_EMC_STATIC_CONFIG_T Static_EMC_Config;

LPC_CCU1->CLKCCU->CFG = (1 << 2) | (1 << 1) | 1;
while (!(LPC_CCU1->CLKCCU->STAT & 1));

if (SystemCoreClock < 80000000UL) {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_0; /* No EMC clock out delay */
}
else {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_2; /* 2.0 ns EMC clock out delay */
}
/*emc pin config*/
LPC_SCU->SFSP[1][0] = EMC_PIN_SET | 2; /* P1_0: A5 */
LPC_SCU->SFSP[1][1] = EMC_PIN_SET | 2; /* P1_1: A6 */
LPC_SCU->SFSP[1][2] = EMC_PIN_SET | 2; /* P1_2: A7 */
LPC_SCU->SFSP[1][3] = EMC_PIN_SET | 3; /* P1_3: OE */
LPC_SCU->SFSP[1][4] = EMC_PIN_SET | 3; /* P1_4: BLS0 */
LPC_SCU->SFSP[1][5] = EMC_PIN_SET | 3; /* P1_5: CS0 */
LPC_SCU->SFSP[1][6] = EMC_PIN_SET | 3; /* P1_6: WE */
LPC_SCU->SFSP[1][7] = EMC_PIN_SET | 3; /* P1_7: D0 */
LPC_SCU->SFSP[1][8] = EMC_PIN_SET | 3; /* P1_8: D1 */
LPC_SCU->SFSP[1][9] = EMC_PIN_SET | 3; /* P1_9: D2 */
LPC_SCU->SFSP[1][10] = EMC_PIN_SET | 3; /* P1_10: D3 */
LPC_SCU->SFSP[1][11] = EMC_PIN_SET | 3; /* P1_11: D4 */
LPC_SCU->SFSP[1][12] = EMC_PIN_SET | 3; /* P1_12: D5 */
LPC_SCU->SFSP[1][13] = EMC_PIN_SET | 3; /* P1_13: D6 */
LPC_SCU->SFSP[1][14] = EMC_PIN_SET | 3; /* P1_14: D7 */

LPC_SCU->SFSP[2][0] = EMC_PIN_SET | 2; /* P2_0: A13 */
LPC_SCU->SFSP[2][1] = EMC_PIN_SET | 2; /* P2_1: A12 */
LPC_SCU->SFSP[2][2] = EMC_PIN_SET | 2; /* P2_2: A11 */
LPC_SCU->SFSP[2][6] = EMC_PIN_SET | 2; /* P2_6: A10 */
LPC_SCU->SFSP[2][7] = EMC_PIN_SET | 3; /* P2_7: A9 */
LPC_SCU->SFSP[2][8] = EMC_PIN_SET | 3; /* P2_8: A8 */
LPC_SCU->SFSP[2][9] = EMC_PIN_SET | 3; /* P2_9: A0 */
LPC_SCU->SFSP[2][10] = EMC_PIN_SET | 3; /* P2_10: A1 */
LPC_SCU->SFSP[2][11] = EMC_PIN_SET | 3; /* P2_11: A2 */
LPC_SCU->SFSP[2][12] = EMC_PIN_SET | 3; /* P2_12: A3 */
LPC_SCU->SFSP[2][13] = EMC_PIN_SET | 3; /* P2_13: A4 */

LPC_SCU->SFSP[5][0] = EMC_PIN_SET | 2; /* P5_0: D12 */
LPC_SCU->SFSP[5][1] = EMC_PIN_SET | 2; /* P5_1: D13 */
LPC_SCU->SFSP[5][2] = EMC_PIN_SET | 2; /* P5_2: D14 */
LPC_SCU->SFSP[5][3] = EMC_PIN_SET | 2; /* P5_3: D15 */
LPC_SCU->SFSP[5][4] = EMC_PIN_SET | 2; /* P5_4: D8 */
LPC_SCU->SFSP[5][5] = EMC_PIN_SET | 2; /* P5_5: D9 */
LPC_SCU->SFSP[5][6] = EMC_PIN_SET | 2; /* P5_6: D10 */
LPC_SCU->SFSP[5][7] = EMC_PIN_SET | 2; /* P5_7: D11 */

LPC_SCU->SFSP[6][3] = EMC_PIN_SET | 3; /* P6_3: CS1 */
LPC_SCU->SFSP[6][6] = EMC_PIN_SET | 1; /* P6_6: BLS1 */

if (SystemCoreClock > 120000000UL) {
LPC_CREG->CREG6 |= (1 << 16);
(LPC_CCU1->CLKCCU[CLK_MX_EMC_DIV].CFG) |= (1 << 5);
}

/* Configure EMC clock-out pins */
LPC_SCU->SFSCLK[0] = EMC_PIN_SET | 0; /* CLK0 */

Static_EMC_Config.ChipSelect = 0;
Static_EMC_Config.Config = (1 < 1) | (1 < 19);
Static_EMC_Config.WaitOen = 0xf;
Static_EMC_Config.WaitPage = 0x1f;
Static_EMC_Config.WaitRd = 0x1f;
Static_EMC_Config.WaitTurn = 0xf;
Static_EMC_Config.WaitWen = 0x2;
Static_EMC_Config.WaitWr = 0x2;

Chip_EMC_Init(1, 0, 0);
Chip_EMC_Enable(1);
Chip_EMC_Static_Init(&Static_EMC_Config);
}

Labels (1)
0 Kudos
Reply
2 Replies

1,415 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Can you tell me the product number of the external NorFlash, and whether you describe what exactly issue you encounter.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,415 Views
cyc583723081
Contributor I

hi,

Thank you for your reply. This problem has been solved.thank you very much.

0 Kudos
Reply