lpc4330 static memory configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc4330 static memory configuration

1,654件の閲覧回数
cyc583723081
Contributor I

How to configure an external static memory controller for lpc4330?I tried to write it, but I didn't succeed.The following is my configuration code,please advise

void Board_ExSram_Init(void)
{
IP_EMC_STATIC_CONFIG_T Static_EMC_Config;

LPC_CCU1->CLKCCU->CFG = (1 << 2) | (1 << 1) | 1;
while (!(LPC_CCU1->CLKCCU->STAT & 1));

if (SystemCoreClock < 80000000UL) {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_0; /* No EMC clock out delay */
}
else {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_2; /* 2.0 ns EMC clock out delay */
}
/*emc pin config*/
LPC_SCU->SFSP[1][0] = EMC_PIN_SET | 2; /* P1_0: A5 */
LPC_SCU->SFSP[1][1] = EMC_PIN_SET | 2; /* P1_1: A6 */
LPC_SCU->SFSP[1][2] = EMC_PIN_SET | 2; /* P1_2: A7 */
LPC_SCU->SFSP[1][3] = EMC_PIN_SET | 3; /* P1_3: OE */
LPC_SCU->SFSP[1][4] = EMC_PIN_SET | 3; /* P1_4: BLS0 */
LPC_SCU->SFSP[1][5] = EMC_PIN_SET | 3; /* P1_5: CS0 */
LPC_SCU->SFSP[1][6] = EMC_PIN_SET | 3; /* P1_6: WE */
LPC_SCU->SFSP[1][7] = EMC_PIN_SET | 3; /* P1_7: D0 */
LPC_SCU->SFSP[1][8] = EMC_PIN_SET | 3; /* P1_8: D1 */
LPC_SCU->SFSP[1][9] = EMC_PIN_SET | 3; /* P1_9: D2 */
LPC_SCU->SFSP[1][10] = EMC_PIN_SET | 3; /* P1_10: D3 */
LPC_SCU->SFSP[1][11] = EMC_PIN_SET | 3; /* P1_11: D4 */
LPC_SCU->SFSP[1][12] = EMC_PIN_SET | 3; /* P1_12: D5 */
LPC_SCU->SFSP[1][13] = EMC_PIN_SET | 3; /* P1_13: D6 */
LPC_SCU->SFSP[1][14] = EMC_PIN_SET | 3; /* P1_14: D7 */

LPC_SCU->SFSP[2][0] = EMC_PIN_SET | 2; /* P2_0: A13 */
LPC_SCU->SFSP[2][1] = EMC_PIN_SET | 2; /* P2_1: A12 */
LPC_SCU->SFSP[2][2] = EMC_PIN_SET | 2; /* P2_2: A11 */
LPC_SCU->SFSP[2][6] = EMC_PIN_SET | 2; /* P2_6: A10 */
LPC_SCU->SFSP[2][7] = EMC_PIN_SET | 3; /* P2_7: A9 */
LPC_SCU->SFSP[2][8] = EMC_PIN_SET | 3; /* P2_8: A8 */
LPC_SCU->SFSP[2][9] = EMC_PIN_SET | 3; /* P2_9: A0 */
LPC_SCU->SFSP[2][10] = EMC_PIN_SET | 3; /* P2_10: A1 */
LPC_SCU->SFSP[2][11] = EMC_PIN_SET | 3; /* P2_11: A2 */
LPC_SCU->SFSP[2][12] = EMC_PIN_SET | 3; /* P2_12: A3 */
LPC_SCU->SFSP[2][13] = EMC_PIN_SET | 3; /* P2_13: A4 */

LPC_SCU->SFSP[5][0] = EMC_PIN_SET | 2; /* P5_0: D12 */
LPC_SCU->SFSP[5][1] = EMC_PIN_SET | 2; /* P5_1: D13 */
LPC_SCU->SFSP[5][2] = EMC_PIN_SET | 2; /* P5_2: D14 */
LPC_SCU->SFSP[5][3] = EMC_PIN_SET | 2; /* P5_3: D15 */
LPC_SCU->SFSP[5][4] = EMC_PIN_SET | 2; /* P5_4: D8 */
LPC_SCU->SFSP[5][5] = EMC_PIN_SET | 2; /* P5_5: D9 */
LPC_SCU->SFSP[5][6] = EMC_PIN_SET | 2; /* P5_6: D10 */
LPC_SCU->SFSP[5][7] = EMC_PIN_SET | 2; /* P5_7: D11 */

LPC_SCU->SFSP[6][3] = EMC_PIN_SET | 3; /* P6_3: CS1 */
LPC_SCU->SFSP[6][6] = EMC_PIN_SET | 1; /* P6_6: BLS1 */

if (SystemCoreClock > 120000000UL) {
LPC_CREG->CREG6 |= (1 << 16);
(LPC_CCU1->CLKCCU[CLK_MX_EMC_DIV].CFG) |= (1 << 5);
}

/* Configure EMC clock-out pins */
LPC_SCU->SFSCLK[0] = EMC_PIN_SET | 0; /* CLK0 */

Static_EMC_Config.ChipSelect = 0;
Static_EMC_Config.Config = (1 < 1) | (1 < 19);
Static_EMC_Config.WaitOen = 0xf;
Static_EMC_Config.WaitPage = 0x1f;
Static_EMC_Config.WaitRd = 0x1f;
Static_EMC_Config.WaitTurn = 0xf;
Static_EMC_Config.WaitWen = 0x2;
Static_EMC_Config.WaitWr = 0x2;

Chip_EMC_Init(1, 0, 0);
Chip_EMC_Enable(1);
Chip_EMC_Static_Init(&Static_EMC_Config);
}

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,459件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Can you tell me the product number of the external NorFlash, and whether you describe what exactly issue you encounter.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,459件の閲覧回数
cyc583723081
Contributor I

hi,

Thank you for your reply. This problem has been solved.thank you very much.

0 件の賞賛
返信