lpc4330 static memory configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc4330 static memory configuration

1,634 次查看
cyc583723081
Contributor I

How to configure an external static memory controller for lpc4330?I tried to write it, but I didn't succeed.The following is my configuration code,please advise

void Board_ExSram_Init(void)
{
IP_EMC_STATIC_CONFIG_T Static_EMC_Config;

LPC_CCU1->CLKCCU->CFG = (1 << 2) | (1 << 1) | 1;
while (!(LPC_CCU1->CLKCCU->STAT & 1));

if (SystemCoreClock < 80000000UL) {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_0; /* No EMC clock out delay */
}
else {
LPC_SCU->EMCDELAYCLK = EMC_CLK_DLY_TIM_2; /* 2.0 ns EMC clock out delay */
}
/*emc pin config*/
LPC_SCU->SFSP[1][0] = EMC_PIN_SET | 2; /* P1_0: A5 */
LPC_SCU->SFSP[1][1] = EMC_PIN_SET | 2; /* P1_1: A6 */
LPC_SCU->SFSP[1][2] = EMC_PIN_SET | 2; /* P1_2: A7 */
LPC_SCU->SFSP[1][3] = EMC_PIN_SET | 3; /* P1_3: OE */
LPC_SCU->SFSP[1][4] = EMC_PIN_SET | 3; /* P1_4: BLS0 */
LPC_SCU->SFSP[1][5] = EMC_PIN_SET | 3; /* P1_5: CS0 */
LPC_SCU->SFSP[1][6] = EMC_PIN_SET | 3; /* P1_6: WE */
LPC_SCU->SFSP[1][7] = EMC_PIN_SET | 3; /* P1_7: D0 */
LPC_SCU->SFSP[1][8] = EMC_PIN_SET | 3; /* P1_8: D1 */
LPC_SCU->SFSP[1][9] = EMC_PIN_SET | 3; /* P1_9: D2 */
LPC_SCU->SFSP[1][10] = EMC_PIN_SET | 3; /* P1_10: D3 */
LPC_SCU->SFSP[1][11] = EMC_PIN_SET | 3; /* P1_11: D4 */
LPC_SCU->SFSP[1][12] = EMC_PIN_SET | 3; /* P1_12: D5 */
LPC_SCU->SFSP[1][13] = EMC_PIN_SET | 3; /* P1_13: D6 */
LPC_SCU->SFSP[1][14] = EMC_PIN_SET | 3; /* P1_14: D7 */

LPC_SCU->SFSP[2][0] = EMC_PIN_SET | 2; /* P2_0: A13 */
LPC_SCU->SFSP[2][1] = EMC_PIN_SET | 2; /* P2_1: A12 */
LPC_SCU->SFSP[2][2] = EMC_PIN_SET | 2; /* P2_2: A11 */
LPC_SCU->SFSP[2][6] = EMC_PIN_SET | 2; /* P2_6: A10 */
LPC_SCU->SFSP[2][7] = EMC_PIN_SET | 3; /* P2_7: A9 */
LPC_SCU->SFSP[2][8] = EMC_PIN_SET | 3; /* P2_8: A8 */
LPC_SCU->SFSP[2][9] = EMC_PIN_SET | 3; /* P2_9: A0 */
LPC_SCU->SFSP[2][10] = EMC_PIN_SET | 3; /* P2_10: A1 */
LPC_SCU->SFSP[2][11] = EMC_PIN_SET | 3; /* P2_11: A2 */
LPC_SCU->SFSP[2][12] = EMC_PIN_SET | 3; /* P2_12: A3 */
LPC_SCU->SFSP[2][13] = EMC_PIN_SET | 3; /* P2_13: A4 */

LPC_SCU->SFSP[5][0] = EMC_PIN_SET | 2; /* P5_0: D12 */
LPC_SCU->SFSP[5][1] = EMC_PIN_SET | 2; /* P5_1: D13 */
LPC_SCU->SFSP[5][2] = EMC_PIN_SET | 2; /* P5_2: D14 */
LPC_SCU->SFSP[5][3] = EMC_PIN_SET | 2; /* P5_3: D15 */
LPC_SCU->SFSP[5][4] = EMC_PIN_SET | 2; /* P5_4: D8 */
LPC_SCU->SFSP[5][5] = EMC_PIN_SET | 2; /* P5_5: D9 */
LPC_SCU->SFSP[5][6] = EMC_PIN_SET | 2; /* P5_6: D10 */
LPC_SCU->SFSP[5][7] = EMC_PIN_SET | 2; /* P5_7: D11 */

LPC_SCU->SFSP[6][3] = EMC_PIN_SET | 3; /* P6_3: CS1 */
LPC_SCU->SFSP[6][6] = EMC_PIN_SET | 1; /* P6_6: BLS1 */

if (SystemCoreClock > 120000000UL) {
LPC_CREG->CREG6 |= (1 << 16);
(LPC_CCU1->CLKCCU[CLK_MX_EMC_DIV].CFG) |= (1 << 5);
}

/* Configure EMC clock-out pins */
LPC_SCU->SFSCLK[0] = EMC_PIN_SET | 0; /* CLK0 */

Static_EMC_Config.ChipSelect = 0;
Static_EMC_Config.Config = (1 < 1) | (1 < 19);
Static_EMC_Config.WaitOen = 0xf;
Static_EMC_Config.WaitPage = 0x1f;
Static_EMC_Config.WaitRd = 0x1f;
Static_EMC_Config.WaitTurn = 0xf;
Static_EMC_Config.WaitWen = 0x2;
Static_EMC_Config.WaitWr = 0x2;

Chip_EMC_Init(1, 0, 0);
Chip_EMC_Enable(1);
Chip_EMC_Static_Init(&Static_EMC_Config);
}

标签 (1)
0 项奖励
回复
2 回复数

1,439 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Can you tell me the product number of the external NorFlash, and whether you describe what exactly issue you encounter.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,439 次查看
cyc583723081
Contributor I

hi,

Thank you for your reply. This problem has been solved.thank you very much.

0 项奖励
回复