lpc177x PWM header files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc177x PWM header files

1,380件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chris_williams_uk on Tue Feb 24 10:49:10 MST 2015
Sorry for a silly question BUT,

My copy of LPCopen does not have header files for the PWM peripherals (and I could not find them in the latest release)!

My chip_lpc177x_8x.h has the definitions:

#define LPC_PWM0_BASE             0x40014000
#define LPC_PWM1_BASE             0x40018000

which look correct, but they are not referenced anywhere! There is no

#define LPC_PWM0 ...

in any of the files on my system.

I see from a previous question that others are using the PWM, so where have you got the files from?

Thanks in advance from someone who is very confuse!

Chris.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,357件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chris_williams_uk on Tue Feb 24 10:59:17 MST 2015
FANTASTIC. Thanks so much.

And yes, I should have been able to find that my self!

Regards,

Chris.
0 件の賞賛
返信

1,357件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Feb 24 10:56:25 MST 2015
See: http://www.lpcware.com/content/forum/lpcopen-pwm-driver
0 件の賞賛
返信