Ethernet Firmware Update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Firmware Update

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hcanova on Mon Nov 02 09:36:48 MST 2015
Hi,

I have made an aplication using FreeRTOS and ethernet comunication on the LPCXpresso 1769 and is working well, but sometimes I need to made some firmware modifications, and I want to do this using the same ethernet conection I'm using to comunicate to the external world.

I found an aplication notes (https://www.lpcware.com/system/files/AN10744_0.pdf) exaplaning how to use the ethernet secondary bootloader with the LPC23xx series. Is possible to use the similar code on the LPC1769?

This aplication notes come with the Ethernet Flash Utility software but only the LPC2xx Devices are avaliable, the source code of this program is Available to download?

The ideia is to have in the future an personalized software to send the firmware to the device maybe in python.

Thansk I lot.

HCanova

ラベル(1)
0 件の賞賛
返信
0 返答(返信)