lpc1768 EXTINT interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1768 EXTINT interface

ソリューションへジャンプ
2,874件の閲覧回数
Sukumar_M
Contributor I

Hi,

I Try to config ir sensor in lpc1768 but it produce unwanted ripples so if i check the output connection should be active how to deactivated the output pin.

 

0 件の賞賛
返信
1 解決策
2,864件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the uart can transmit irDa signal from it's Uartx_TX pin, which is a bit stream modulated by the 38KHz signal, the 38khz fixed duty cycle signal can be generated by uart module itself. If you want LPC uart_rx pin to receive the irDa signal, I suppose that you have to create an analog low-pass filter circuit to remove the 38K modulated signal, then use uart_RX pin to receive the filtered data stream.

For the EXTINT pin, it is an input pin, which can accept external signal to fire interrupt.

If I misunderstand you, I am sorry.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,865件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the uart can transmit irDa signal from it's Uartx_TX pin, which is a bit stream modulated by the 38KHz signal, the 38khz fixed duty cycle signal can be generated by uart module itself. If you want LPC uart_rx pin to receive the irDa signal, I suppose that you have to create an analog low-pass filter circuit to remove the 38K modulated signal, then use uart_RX pin to receive the filtered data stream.

For the EXTINT pin, it is an input pin, which can accept external signal to fire interrupt.

If I misunderstand you, I am sorry.

BR

XiangJun Rong

0 件の賞賛
返信
2,860件の閲覧回数
Sukumar_M
Contributor I

But EXTINT also use For an Counting purpose

0 件の賞賛
返信
2,856件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you want to count external clock number, you can connect the external clock signal to the Timer Capx pin, by proper configuration, the Timer will count the number of external clock signal.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信