lpc1347 could not connect to core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1347 could not connect to core

ソリューションへジャンプ
2,427件の閲覧回数
mateuszkiełbasa
Contributor III

I started my adventure with cortex m3 on lpc137. I have big problem. Suddenly I cant flash my board with errror "Failed to connect Ee(36). Could not connect to core".

Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink.exe build 725)
Pc: ( 0) Reading remote configuration
Pc: ( 5) Remote configuration complete
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'
Nc: probe unbooted? no core 0?
Ed:02: Failed on connect: Ee(36). Could not connect to core.
Et:31: No connection to emulator device
Pc: (100) Target Connection Failed

I am confused... I am scared I broke my board... Can someone help me?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
mateuszkiełbasa
Contributor III

EDIT

I reset board with this tutorial: https://community.nxp.com/message/630748 . It helps!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,928件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below threads and let me know if this helps!!

Could not connect to core | www.LPCware.com 

Failed on connect: Ee(XX). Could not connect to core. | www.LPCware.com 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,929件の閲覧回数
mateuszkiełbasa
Contributor III

EDIT

I reset board with this tutorial: https://community.nxp.com/message/630748 . It helps!

0 件の賞賛
返信