lpc 433x DFU script for RASPBERRY 3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc 433x DFU script for RASPBERRY 3

ソリューションへジャンプ
2,339件の閲覧回数
vianneyfenart
Contributor II

Hello,

I want upload bin file from RASPBERRY 3 (RASPBIAN) to LPC433X ARM processor in dfu mode.

I can do that easily with dfusec utility on Windows but i can't find the equivalent for a ARM LINUX OS...

Have you got solution?

thanks

ラベル(2)
1 解決策
2,192件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

元の投稿で解決策を見る

2 返答(返信)
2,192件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

2,192件の閲覧回数
vianneyfenart
Contributor II

Thanks for your help!

0 件の賞賛
返信