lpc 433x DFU script for RASPBERRY 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc 433x DFU script for RASPBERRY 3

Jump to solution
2,339 Views
vianneyfenart
Contributor II

Hello,

I want upload bin file from RASPBERRY 3 (RASPBIAN) to LPC433X ARM processor in dfu mode.

I can do that easily with dfusec utility on Windows but i can't find the equivalent for a ARM LINUX OS...

Have you got solution?

thanks

Labels (2)
1 Solution
2,192 Views
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

View solution in original post

2 Replies
2,192 Views
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

2,192 Views
vianneyfenart
Contributor II

Thanks for your help!

0 Kudos
Reply