lpc 1347 using built-in functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc 1347 using built-in functions

1,390 Views
mateuszkiełbasa
Contributor III

I just started my adventure with microcontrollers. I am working on lpc 1347. There is many functions used in examples (for example Board_LED_Toggle(), Chip_ADC_Read_Value() etc.). Where I can find its documentation or manual? I have lpc1347 reference manual. My second question is what I should learn first? Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,166 Views
soledad
NXP Employee
NXP Employee

Hello Mateusz,

You can use the following doc as reference How to create a new LPC project using LPCOpen and LPCXpresso 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply