lpc 1347 using built-in functions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc 1347 using built-in functions

1,429件の閲覧回数
mateuszkiełbasa
Contributor III

I just started my adventure with microcontrollers. I am working on lpc 1347. There is many functions used in examples (for example Board_LED_Toggle(), Chip_ADC_Read_Value() etc.). Where I can find its documentation or manual? I have lpc1347 reference manual. My second question is what I should learn first? Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,205件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Mateusz,

You can use the following doc as reference How to create a new LPC project using LPCOpen and LPCXpresso 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信