library is a ported of the emwin for lpc1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

library is a ported of the emwin for lpc1768

1,926 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Wed Oct 22 02:10:23 MST 2014
hi
i have a landtiger board for lpc1768.
Lcd specification:
(

Resolution:  QVGA 262K 240*RGB*320
Size: 3.2"
Controller: IL9320
Touch Panel: 4-wire
Pin Pitch: 37Pins & 1mm
2.7-3.3V operating voltage
Backlight: 5 LEDs Parallel
RSM1843 touch panel controller onboard  directly compatible with ADS7843
Standard 2.54mm PCB headers for prototyping
Support a SD card interface
)
Someone have ported library's emwin for this board?
thnks!
标签 (1)
0 项奖励
回复
3 回复数

1,456 次查看
gui_builder
Contributor I

hello ,

the link is broken. is it possible to give another link for the tutorial on how to import seggers emWin in LPC1768 with keil .

thanks in advance

0 项奖励
回复

1,766 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Fri Oct 24 10:09:21 MST 2014
thank you
I've Previously seen this file
Wanted to see if someone did not ported this library for landtiger?
Notifying me
0 项奖励
回复

1,766 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Oct 24 08:57:47 MST 2014
Hi engineer1,
Porting guide on below link may be helpful.
http://www.lpcware.com/content/nxpfile/emwin-porting-guide-ea-lpc1788-bsp-keil-mcb1700-english-versi...
0 项奖励
回复