lgdp4525 with 8 bit interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lgdp4525 with 8 bit interface

1,140件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hugo12 on Thu Aug 07 09:06:05 MST 2014
Hi everybody,

i have some problems with my custom board. I am using a lpc1765 and a 2" display with a lgdp4525 connected via 8 bit interface. The 4525 is similar to the lgdp4531, so i am using the flexcolor driver. After reading the porting guide and  adapting the code the display seems to work but not correctly. When trying to run "Hello World!" there are only some lines of pixels appearing (see attached picture). Changing the background color for example works fine.
Has anyone hints for me to find the problem?

Thank you.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)