lgdp4525 with 8 bit interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lgdp4525 with 8 bit interface

1,139 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hugo12 on Thu Aug 07 09:06:05 MST 2014
Hi everybody,

i have some problems with my custom board. I am using a lpc1765 and a 2" display with a lgdp4525 connected via 8 bit interface. The 4525 is similar to the lgdp4531, so i am using the flexcolor driver. After reading the porting guide and  adapting the code the display seems to work but not correctly. When trying to run "Hello World!" there are only some lines of pixels appearing (see attached picture). Changing the background color for example works fine.
Has anyone hints for me to find the problem?

Thank you.
Labels (1)
0 Kudos
Reply
0 Replies