jump using blhost

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

jump using blhost

跳至解决方案
3,131 次查看
embedded_eng_
Contributor III

Hi,

Im using blhost to jump to my image (execute).

the first 8 bytes of my bin file are: 00 00 01 20 71 01 00 00

So my command is:

./blhost -u 0x1fc9,0x0022 execute 0x00000171 0 0x20010000

Now, I've noticed that it will work with every address I pass to the command, for example:

./blhost -u 0x1fc9,0x0022 execute 0xaaaaaaaa 0 0x20010000

Why?

What is the correct way to do it?

标记 (3)
0 项奖励
回复
1 解答
3,029 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

I'm not sure the inside processing of command "execute", I think the reason for "Why does the jump command with an invalid address works as well?" is your image start from 0x00000, so no matter the address is , it always start up from 0x0000, it can work well.

If image start from other address, for example, in mcu, a secondary bootloader +APP module, APP

start from 0x1000, then the <address> should the exactly data as User's Guide said.

Or image is in RAM, also <address> need read from first 8 bytes.

 

BR

Alice

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,070 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

First one is correct.

0 项奖励
回复
3,060 次查看
embedded_eng_
Contributor III

Hi, Thanks for the response.

Why does the jump command with an invalid address works as well?

Any Address that I've tried worked..

The commands fails only when I try a different stack pointer.

Another question: 

Before the jump I'm writing to address 0x00000000, should I write instead to address 0x00000171 (taken from 8 first bytes)?

 

Thanks 

0 项奖励
回复
3,030 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

I'm not sure the inside processing of command "execute", I think the reason for "Why does the jump command with an invalid address works as well?" is your image start from 0x00000, so no matter the address is , it always start up from 0x0000, it can work well.

If image start from other address, for example, in mcu, a secondary bootloader +APP module, APP

start from 0x1000, then the <address> should the exactly data as User's Guide said.

Or image is in RAM, also <address> need read from first 8 bytes.

 

BR

Alice

 

0 项奖励
回复
3,082 次查看
embedded_eng_
Contributor III

Someone?

Before the "execute" command, I'm running:

./blhost -u 0x1fc9,0x0022 write-memory 0x00000000 file.bin

 

0 项奖励
回复