is USB1 VBUS connection required on LPC55S69 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is USB1 VBUS connection required on LPC55S69 ?

1,610件の閲覧回数
hazarm
Contributor I

is USB1 VBUS connection required on LPC55S69? 
can the vbus detected by something else like pd-controller, and usb1 can be turned on by software/pin toggle?

thanks,

h

0 件の賞賛
返信
3 返答(返信)

1,591件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I recommend download the Hardware design guidelines.

Pavel_Hernandez_0-1728671366134.png

Best regards,
Pavel

0 件の賞賛
返信

1,578件の閲覧回数
hazarm
Contributor I
hi pavel,

maybe i wasn't clear with my question. we still want to use usb1 interface.

the problem is it is an usb-pd input so the VBUS is between 5V-20V. we do have pd controller can pull an interrupt when the vbus is connected.

so the question is can we enable the USB1 phy internally without a need for external VBUS.
this is possible with USB0 phy because 3.3V is expected and can be turned on internally.

thanks,
best regards,
hazar
0 件の賞賛
返信

1,528件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I reviwed the information on the Datasheet this may be clear for you.

Pavel_Hernandez_0-1729029516922.png

Best regards,
Pavel

0 件の賞賛
返信