iType font converstion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iType font converstion

1,917件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wendtr on Wed Jun 12 13:55:10 MST 2013

I am using emWin 5.20.  As part of emWin5.20, the iType font generator is included as an option.  In linking in the source code, it is also trying to link in the header file "fs_api.h", which does not exist.  It appears, however, that this file is included with Segger's emFile system, which is not included as part of emWin's LCD license.  This begs the question... can we use iType on LPC's implementation of emWin?  If so, where is this file?

ラベル(1)
0 件の賞賛
返信
1 返信

1,876件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wendtr on Mon Jun 17 16:44:14 MST 2013

Received word from Segger that this feature is only available with emFile installed...

0 件の賞賛
返信