iType font converstion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iType font converstion

1,951 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wendtr on Wed Jun 12 13:55:10 MST 2013

I am using emWin 5.20.  As part of emWin5.20, the iType font generator is included as an option.  In linking in the source code, it is also trying to link in the header file "fs_api.h", which does not exist.  It appears, however, that this file is included with Segger's emFile system, which is not included as part of emWin's LCD license.  This begs the question... can we use iType on LPC's implementation of emWin?  If so, where is this file?

Labels (1)
0 Kudos
Reply
1 Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wendtr on Mon Jun 17 16:44:14 MST 2013

Received word from Segger that this feature is only available with emFile installed...

0 Kudos
Reply