i2c0 fails on port 1 lpc4088

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i2c0 fails on port 1 lpc4088

841 次查看
kennethedlow
Contributor I

When the lpc4088 or lpc4078 is configured to use port 1 pin 30 and 31 for i2c0 the device enters a busy state after the function  tmp = Chip_I2C_MasterSend(I2C0, hdmi_xfer.slaveAddr, hdmi_xfer.txBuff, hdmi_xfer.txSz); is executed.

0 项奖励
回复
1 回复

774 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kenneth,

    When you run the I2C0 code on LPC4088, do you connect it with the according I2C slave device?

    Please check the I2C communication wave, when the master send data, does slave give ACK feed back?


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复