i2c_master_config_t

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c_master_config_t

1,489 Views
JK_265
Contributor III

Can anyone explain how the "enableTimeout" field in this structure is meant to be used:

typedef struct _i2c_master_config
{
bool enableMaster; /*!< Whether to enable master mode. */
uint32_t baudRate_Bps; /*!< Desired baud rate in bits per second. */
bool enableTimeout; /*!< Enable internal timeout function. */
uint8_t timeout_Ms; /*!< Event timeout and SCL low timeout value. */
} i2c_master_config_t;

There does not seem to be much information on it, and the SDK autogenerated code just toggles the initial field from false to true.  I don't see where this field is actually checked in the driver source code.  Am I supposed to register a handler for the timeout, etc...? Or is this a purely hardware item?  What is actually timing out - the clock stretching, a read/write operation, a whole transaction, etc...?

Specifically working with an LPC55S16 if it matters.

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,438 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @JK_265 

The information regarding the timout is on the User manual UM11295, chapter 33.6.2 I2C configuration register, 

Miguel04_0-1696014300130.png

 

Best Regards, Miguel.

0 Kudos
Reply