how to flash LPC54102 board wihtout using lpcexpresso software at the customer end?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to flash LPC54102 board wihtout using lpcexpresso software at the customer end?

2,407件の閲覧回数
chethankumar
Contributor III

Hi,

I am using board which contains LPC54102 chip. I want to update the firmware(newly created axf) of the board without using LPCExpresso IDE. What are the possible solutions available (ex:USB, UART or Wi-Fi)? Can it flashed using script?.

Please point us to the relevant document or any pre-written script.

Thanks,

ck

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,131件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The user manual contains a chapter entitled 'the Flash API' which contains all the information you should need. Alternatively you could look at a tool such as FlashMagic Flash Magic - Welcome . Note you may need to extract the binary from the .axf image.

Yours,

LPCXpresso support

0 件の賞賛
返信

2,131件の閲覧回数
chethankumar
Contributor III

Hi,

Is it possible to program the LPC54102 using LPCScript as suggested by below link

http://www.nxp.com/files/microcontrollers/doc/user_guide/LPCScrypt_User_Guide.pdf?fasp=1&WT_TYPE=Use...
However above link is for  LPC18/43 family. If it is possible to program the LPC54102 also can you provide the necessary script?.

Thanks,
Ck
0 件の賞賛
返信