how do convert a 11u14 program to 1114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how do convert a 11u14 program to 1114

2,591件の閲覧回数
jordanhalgunset
Contributor I

my test board is 11u14

but the project board  is 1114.

Program does not run the same on project board

0 件の賞賛
返信
5 返答(返信)

2,499件の閲覧回数
jordanhalgunset
Contributor I

I was not able to find a driver but was to find the programs i needed.

                thank you,

                 jordan

0 件の賞賛
返信

2,499件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jordan,

   You are welcome!

   Driver is in folder:lpcopen_v2_00a_keil_iar_nxp_lpcxpresso_11c24\software

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,499件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jordan Halgunseth,

    You must change the head file to LPC1114, because LPC11U14 and LPC1114 have some difference. The register address also have difference.

   Please change the head file, then check the driver, you should better use the LPC1114 driver.

  About the LPC1114 driver, you can refer to lpcopen code:

LPCOpen Software for LPC11XX|NXP 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,499件の閲覧回数
jordanhalgunset
Contributor I

I was not able to find the 1114 driver.

Do you know where it is located?

If you have it could you email it me?

    thank you,

     Jordan

0 件の賞賛
返信

2,499件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jordan,

   Can't you find the code from my last post link?

  https://www.nxp.com/downloads/en/software/lpcopen_v2_00a_keil_iar_nxp_lpcxpresso_11c24.zip 

 LPCXpresso LPC11C24 board Supports LPC1111/12/13/14/15/00XL C00/C12/C14/C22/C24/D24 (Does not support 'LPC11xxLV')


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信