hii.!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hii.!

1,285 Views
arthshah
Contributor II

i am working with LPC2148 Development Board. I need VCOM Driver for LPC2148 for Win 10 64 bit.

plz send me driver for it.

0 Kudos
Reply
1 Reply

1,173 Views
b36401
NXP Employee
NXP Employee

Unfortunately we have no such drivers.
Only µC/OS RTOS and embOS RTOS are officially supported with LPC2148.
Sorry for the inconvenience.

Single-chip 16-bit/32-bit microcontrollers; up to 512 kB flash with ISP/IAP, USB 2.0 full-speed devi... 

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply