hii.!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hii.!

829 次查看
arthshah
Contributor II

i am working with LPC2148 Development Board. I need VCOM Driver for LPC2148 for Win 10 64 bit.

plz send me driver for it.

0 项奖励
回复
1 回复

717 次查看
b36401
NXP Employee
NXP Employee

Unfortunately we have no such drivers.
Only µC/OS RTOS and embOS RTOS are officially supported with LPC2148.
Sorry for the inconvenience.

Single-chip 16-bit/32-bit microcontrollers; up to 512 kB flash with ISP/IAP, USB 2.0 full-speed devi... 

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复