hello, i have two LPC2364 placed on a board, i want to connect them via ethernet directly withou using of two physical chip. this is possible and what is solution?thanks in advance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hello, i have two LPC2364 placed on a board, i want to connect them via ethernet directly withou using of two physical chip. this is possible and what is solution?thanks in advance

997 次查看
johnadams
Contributor I

hello, i have two LPC2364 placed on a board,

i want to connect them via Ethernet directly without using of two physical chip.

is it possible? and what is solution?

thanks in advance.

0 项奖励
回复
1 回复

764 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could directly connect both Ethernet devices without a PHY, connecting TX to RX lines and RX to TX lines. For additional details, you could refer to the following Community link:

https://community.nxp.com/thread/316374

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复