example code for usb virtual com port using lpc54628

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

example code for usb virtual com port using lpc54628

2,449 Views
allevato_loris
Contributor I

Dear sirs,

 

I need example code for usb virtual com port to communicate data to pc windows 7.

 

Thanks for the help.

With regards

Loris 

Labels (1)
0 Kudos
Reply
3 Replies

2,335 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Loris Allevato,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd like to recommend you to refer to the USB CDC demos in the SDK library.
SDK download link:
https://mcuxpresso.nxp.com/en/welcome


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,335 Views
allevato_loris
Contributor I

Dear jeremyzhou,

I tried with the 2.5.0 version of the SDK but Windows 7 does not recognize the USB port, do I have to install any driver? If yes where can I find it?

In my application I have to send data (strings) from the board to the pc, it could indicate the most appropriate example from which to start.

Thanks to the availability

With regards

Loris 

0 Kudos
Reply

2,335 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Loris Allevato,

It exists an inf folder in USB CDC demo's directory, and in that folder, it contains the driver file, please check it.

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply