emWin 5.38b compilation settings/multitasking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emWin 5.38b compilation settings/multitasking

2,468 次查看
carstengroen
Senior Contributor II

When downloading emWin 5.38b from: emWin Graphics Library|NXP 

it seems there is no multitasking support included ?!? 

I have a project that needs to run on both a LPC546x (which works fine with multitask support/GUI_OS 1), and on a LPC1788 platform. When downloading the before mentioned 5.38b, it seems that GUI_OS is NOT defined as 1

Is it possible (for NXP) to deliver Cortex M3 emWin library with OS support ??

(needed urgently!)

标签 (3)
0 项奖励
回复
3 回复数

2,247 次查看
soledad
NXP Employee
NXP Employee

Hi,

emWin library is developed by our partner SEGGER. Unfortunately we cannot to deliver a library like you need.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,247 次查看
carstengroen
Senior Contributor II

Sol.

this is not quite how it works if I'm not mistaken ?

According to Segger, it is NXP (and other chip vendors which also delivers emWin for their products) who builds the lib files based on the compile switches (defines) for each of the variants. This also fits fine with the fact that the M4 version (for LPC546x) has been built with RTOS support. For some reason the M3 version NXP delivers has not been built with RTOS support.

As I wrote, according to Segger it is NXP that makes the decision which defines to use when building

(this also does not answer why the versions NXP makes available are more than 2 years "outdated" ?) 

0 项奖励
回复

2,247 次查看
carstengroen
Senior Contributor II

Care to comment on this ?

(Its no problem for us any longer, we went with another provider for this, but others might have the same problem..)

0 项奖励
回复