dual boot: SPIFI-image programming, running from internal Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

dual boot: SPIFI-image programming, running from internal Flash

2,206 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Bernardo on Tue Aug 27 23:33:28 MST 2013
We are using an LPC1822 together with a Spansion S25F128 or S25F256 quad-SPI. The setup is:

> Internal Flash is used for main application and for programming an image into SPIFI-flash.
> SPIFI-program used for testing purposes, incorporating boot loader for updating software in internal flash.
> Development platform LPCXpresso.

What steps are needed to program an application image into the mentioned SPIFI-chip,
by a program running from internal flash?
标签 (1)
0 项奖励
回复
2 回复数

2,157 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Donna111 on Thu Oct 24 01:05:33 MST 2013
HI there
For me ,i usually programing an image using this image programing tool.You can take a look.
There is detailed tutorial .Hope to help you.
0 项奖励
回复

2,156 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Sun Oct 20 12:59:12 MST 2013
Hi, Bernardo,

The LPCXpresso IDE allows you to program the SPIFI-Chip.

I have attached a screen shot of the location of this tool.



0 项奖励
回复