dsbl image_generator.exe not working with ram functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

dsbl image_generator.exe not working with ram functions

877 次查看
jfchenier
Contributor I

Hello,

I am trying to integrate the dsbl bootlaoder to our project, but the image_generator.exe program doesn't work on our code. I have been able to pinpoint the problem. It seems that the program doesn't like the fact that our linker script load .text element in RAM to save on power and wait states. Is there a place where the source code of this is available? It is also not super convenient that the program works only on Windows. 

Thank you. 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

847 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jfchenier 

Do you ask the source code of "image_generator.exe" tool?

If yes, you can take a personal service ticket: 

https://support.nxp.com/s/?language=en_US 

 

BR

Alice