dsbl image_generator.exe not working with ram functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dsbl image_generator.exe not working with ram functions

1,227 Views
jfchenier
Contributor I

Hello,

I am trying to integrate the dsbl bootlaoder to our project, but the image_generator.exe program doesn't work on our code. I have been able to pinpoint the problem. It seems that the program doesn't like the fact that our linker script load .text element in RAM to save on power and wait states. Is there a place where the source code of this is available? It is also not super convenient that the program works only on Windows. 

Thank you. 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,197 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jfchenier 

Do you ask the source code of "image_generator.exe" tool?

If yes, you can take a personal service ticket: 

https://support.nxp.com/s/?language=en_US 

 

BR

Alice