difference between FIODIR & IODIR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

difference between FIODIR & IODIR

4,575件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moslem1368 on Sun Dec 02 02:59:49 MST 2012
Hi
What is difference between FIODIR &  IODIR Reg. in lpc21xx in Aplication?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,994件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Aug 15 15:50:45 MST 2013
Hi,

FIODIR refers to Fast Input/Output Direction control register and IODIR refers to Input/Output Direction control register. The purpose of FIO is basically application oriented. In case you have a external memory running at high frequencies and you want to communicate with it. Here, FIO's are better than IO's as they are faster.

Thanks,
SK
0 件の賞賛
返信

3,994件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by omid.azadeh on Mon Apr 08 01:43:57 MST 2013

hi


FIODIR -> Fast Input/Output Direction


IODIR -> Normally Input/Output Direction

0 件の賞賛
返信