dfu_composite and periph_iram_blinky examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dfu_composite and periph_iram_blinky examples

879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by toad on Fri May 16 08:49:24 MST 2014
hardware: hitex 4350
toolset: Kiel MDK-5
software: lpc_open_209

I download the periph_iram_blinky example via dfu to the board running dfu_composite example, when the periph_iram_blinky example is executed it causes a HardFault, during the setting up of the clocks. If I remove the call to SetupClocks from the iram_blinky image it works. So my question, should the dfu_composite example not be reverting the clocks back to a base configuration before jumping to the reset handler ? Thanks.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)