dLAN Green PHY eval board II - help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dLAN Green PHY eval board II - help

20,689件の閲覧回数
andrearendine
Contributor II

Hi everyone, 

I have two dLAN PHY eval board useful for powerline communication and I'd like to understand better how to programm this board based on LPC1758. 

If someone have a detailed documentation (more that the datasheed and manual on the website of Devolo which are very poor writed) or some examples about this board could be great. 

I'd like, just to start, to send a paket via PLC e and turn on the LED to the other board. 

Thanks 

Andrea 

ラベル(5)
タグ(5)
23 返答(返信)

9,602件の閲覧回数
tobiasfrauenrat
Contributor I

Dear Andrea, 

devolo provides a new SDK, which is available on github.  

GitHub - devolo/dlan-greenphy-sdk: The devolo dLAN Green PHY module is ideal for installation in all... 

This SDK is under development and there is no MQTT included yet, but it should be easy to start with this software, because it is more structured and FreeRTOS 9 is included. Please checkout the 'devolop' branch for the moment.

Best regards, Tobias.

0 件の賞賛
返信

9,304件の閲覧回数
carlovalgocela
Contributor III

Hello tobiasfrauenrath

Do you have any updated documents and SDK?

I wanted to add more functions like PWM and ADC.

0 件の賞賛
返信

1,489件の閲覧回数
andrearendine
Contributor II

Hi Tobias,

I'm beginning of this stuff on Devolo so I'd like to have somethig which

explain kind of detail how to start with this board.

I have the board, the debug, the IDE for programming, but actually I

didn't found a guide on how to use this evaluation board. ( how to

connect? how to flash the firmware? how does works the libraries? how does

is handled the HOME PLUG POWERLINE? etc..)

Also an electronic schematic about this could be interesting to have.

Can you help me?

Thanks

Andrea Rendine

R&D dept.

Meta System S.p.A.

Soggetta a direzione e coordinamento della società Shenzhen Deren

Electronic CO., LTD

www.metasystem.it

Via Galimberti 9

42124 - Reggio Emilia

Tel:0522364267

[email protected]

Da: tobiasfrauenrath <[email protected]>

Per: Andrea Rendine <[email protected]>,

Data: 12/05/2017 14:41

Oggetto: Re: - Re: dLAN Green PHY eval board II - help

NXP Community

Re: dLAN Green PHY eval board II - help

reply from Tobias Frauenrath in LPC - View the full discussion

Dear Andrea,

devolo provides a new SDK, which is available on github.

GitHub - devolo/dlan-greenphy-sdk: The devolo dLAN Green PHY module is

ideal for installation in all IoT-devices. Inclu?

This SDK is under development and there is no MQTT included yet, but it

should be easy to start with this software, because it is more structured

and FreeRTOS 9 is included. Please checkout the 'devolop' branch for the

moment.

Best regards, Tobias.

Reply to this message by replying to this email, or go to the message on

NXP Community

Start a new discussion in LPC by email or at NXP Community

Following Re: dLAN Green PHY eval board II - help in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email

frequency in your email preferences

Il contenuto di questo messaggio elettronico e' riservato ed e' rivolto esclusivamente al/ai destinatario/i identificato/i. Pertanto e' proibito leggerlo, copiarlo, divulgarlo o utilizzarlo da parte di chiunque salvo il/i destinatario/i. Se non siete il destinatario, vi invitiamo a cancellare il messaggio ed eventuali allegati dandocene immediatamente comunicazione scritta a mezzo posta elettronica. Sebbene la società mittente si impegna ad assumere tutte le misure più idonee per assicurare l'assenza di virus all'interno di eventuali allegati alla presente comunicazione e-mail, tali misure non costituiscono una garanzia assoluta e pertanto vi invitiamo a porre in essere i vostri controlli antivirus prima di aprire qualsiasi allegato. La società mittente non si assume alcuna responsabilità per eventuali danni che potreste subire a causa di virus sul software.

This e-mail and any attachment are confidential and intended for the addressee(s) only. Reading, copying, disclosure or use by anybody else is unauthorized. If you are not the intended recipient, please delete this message and any attachment and advise the sender by return e-mail. Whilst the sender company takes reasonable care to ensure that any attachment to this e-mail does not contain software viruses, this cannot be guaranteed and you should therefore carry out your own virus checks before opening any attachment. The sender company accepts no responsibility or liability for any damage that you may suffer as a result of software viruses.

0 件の賞賛
返信