bit 0 LPC_CGU->PLL1_STAT change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bit 0 LPC_CGU->PLL1_STAT change

1,347 Views
gustavomuro
Contributor I

Hi

When the processor start, the bit 0 of LPC_CGU->PLL1_STAT change betwen 1 and 0.

This cause the function Chip_Clock_GetRate(CLK_MX_MXCORE) return 0 because Chip_Clock_GetMainPLLHz() return 0.

What time recommend waiting for it to stabilize?

Thanks!

Labels (2)
0 Kudos
Reply
1 Reply

1,247 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gustavo,

   Could you please tell us what the chip you are using now?

   Then we can help you to check it or find a code for your reference .

Waiting for your reply!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply