X-loader LPC3250 embedded artists

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

X-loader LPC3250 embedded artists

1,014件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abadou on Thu Feb 28 14:56:07 MST 2013
Hi, I have started working on LPC3250 embedded artists
I plugged the card with the PC (windows 7) but in hyperterminal (TeraTerm). I do not see the launch of x-loader (stored by default in the map), I do not know the source of the problem
is that the card is only compatible with Windows XP??
I do not know how can I resolve this problem ??
help me plzzz
ラベル(1)
0 件の賞賛
返信
0 返答(返信)