Windows USB driver for LPC1549

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows USB driver for LPC1549

4,393 次查看
isaotakashima
Contributor IV

We will develop some USB device such as USB to serial, USB Keyboard using LPC1549.

I'm looking for Windows 8.1 and 10 USB driver NXP home page.

I find the "LPCXpresso Link2 USB driver package(REV 2.0.2)" at below link.

https://www.nxp.com/downloads/en/software/lpc_driver_setup.exe 

Can we these USB driver for our USB device?

If no, please tell us correct link address for it.

Please advise as soon as possible.

Best regards,

Takashima

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

3,966 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Isao,

Pls refer to the link:

LPC-Link2 | NXP 

The LPCXpresso Link2 USB driver package is run on the LPC4370 which is integrated on the LPC-LINK2 board, the LPC-LINK2 board can be configured to support various development tools and IDEs using a variety of different downloadable firmware images, the firmware image is the ./lpc_driver_setup.exe

I suppose we have not the usb driver run the PC side based on win8.1. But on the USB example in SDK package, there are some applications run on the PC side which is just used to demo the communication with the LPC usb port either as host or device.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复