Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

1,912 Views
seanzhou
Contributor II

Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

Sometimes, we can update the firmware by other file names, such as 1.bin, abc.bin, firmware1.bin...etc.

Sometimes we will fail. And found that all flash memory is 0xFFFFFFFF.

What are the rules for LPC546xx ISP mass storage firmware update?

Labels (1)
0 Kudos
Reply
3 Replies

1,788 Views
seanzhou
Contributor II

Thanks, This information has been passed on to others.

0 Kudos
Reply

1,779 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @seanzhou 

Thanks for the update !

If I can help you further let me know.

Diego.

( If you consider my previous reply as the solution , you can  mark it down)

0 Kudos
Reply

1,899 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @seanzhou 

In this case the  .bin should be named firmware.bin only :

Please take a look at this excerpt from the chapter 3.1 Loading applications using USB mass storage boot (MSC class) mode (LPCXpresso546x8 boards only) from the LPCXpresso546x8/540xx/54S0xx Board User Manual:

 

4. Drag and drop the new binary file to the drive. Note that this new file must have the name firmware.bin, otherwise the file seems to be transferred and program but in fact it is not.

 

Best regards,

Diego.