Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

1,915件の閲覧回数
seanzhou
Contributor II

Why is LPC546xx ISP mass storage stable only when the file name is firmware.bin?

Sometimes, we can update the firmware by other file names, such as 1.bin, abc.bin, firmware1.bin...etc.

Sometimes we will fail. And found that all flash memory is 0xFFFFFFFF.

What are the rules for LPC546xx ISP mass storage firmware update?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,791件の閲覧回数
seanzhou
Contributor II

Thanks, This information has been passed on to others.

0 件の賞賛
返信

1,782件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @seanzhou 

Thanks for the update !

If I can help you further let me know.

Diego.

( If you consider my previous reply as the solution , you can  mark it down)

0 件の賞賛
返信

1,902件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @seanzhou 

In this case the  .bin should be named firmware.bin only :

Please take a look at this excerpt from the chapter 3.1 Loading applications using USB mass storage boot (MSC class) mode (LPCXpresso546x8 boards only) from the LPCXpresso546x8/540xx/54S0xx Board User Manual:

 

4. Drag and drop the new binary file to the drive. Note that this new file must have the name firmware.bin, otherwise the file seems to be transferred and program but in fact it is not.

 

Best regards,

Diego.