Which emWin should I use for LPC4088

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which emWin should I use for LPC4088

1,330 Views
mikemillsap
Contributor I

I have the LPC4088 processor with 7" touch LCD. We plan to use emWin to develop a GUI interface for a project. I am currently working with version 5.22, but I see newer ones available on the NXP site. Should I download the latest?

It appears that 5.30c is available, is it compatible with LPC4088?

Also, do I have to download these libraries from NXP or can I go to the Segger site directly?

Thanks!

0 Kudos
Reply
1 Reply

1,231 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The latest emWin V5.30c supports LPC4088 product.

I would recommend customer to download emWIN software for NXP product from NXP emWin website.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply