SSP DMA, rx buffer stays empty

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SSP DMA, rx buffer stays empty

1,817件の閲覧回数
gvandenbosch
Contributor I

Hello,

I am trying to get the SSP running with DMA on the LPC4357.

For this I configured 1 DMA channel for TX and 1 DMA channel for RX.

However the RX buffer always stays empty.

I have configured the DMA as following:

NVIC_DisableIRQ(DMA_IRQn);

NVIC_SetPriority(DMA_IRQn, ((0x01 << 3) | 0x01));

GPDMA_Init();

GPDMA_Channel_CFG_Type dma_txconfig;

dma_txconfig.ChannelNum = 0;

dma_txconfig.TransferSize = n;

dma_txconfig.TransferWidth = GPDMA_WIDTH_BYTE;

dma_txconfig.SrcMemAddr = (uint32_t)&txbuf;

dma_txconfig.DstMemAddr = 0;

dma_txconfig.TransferType = GPDMA_TRANSFERTYPE_M2P_CONTROLLER_DMA;

dma_txconfig.SrcConn = 0;

dma_txconfig.DstConn = GPDMA_CONN_SSP1_Tx;

dma_txconfig.DMALLI = 0;

GPDMA_Setup(&dma_txconfig);

GPDMA_Channel_CFG_Type dma_rxconfig;

dma_rxconfig.ChannelNum = 1;

dma_rxconfig.TransferSize = n;

dma_rxconfig.TransferWidth = GPDMA_WIDTH_BYTE;

dma_rxconfig.SrcMemAddr = 0;

dma_rxconfig.DstMemAddr = (uint32_t)&rxbuf;

dma_rxconfig.TransferType = GPDMA_TRANSFERTYPE_P2M_CONTROLLER_DMA;

dma_rxconfig.SrcConn = GPDMA_CONN_SSP1_Rx;

dma_rxconfig.DstConn = 0;

dma_rxconfig.DMALLI = 0;

GPDMA_Setup(&dma_rxconfig);

Channel0_TC = 0;

Channel0_Err = 0;

Channel1_TC = 0;

Channel1_Err = 0;

NVIC_EnableIRQ(DMA_IRQn);

GPDMA_ChannelCmd(0, ENABLE);

SSP_DMACmd(spip->ssp, SSP_DMA_TX, ENABLE);

GPDMA_ChannelCmd(1, ENABLE);

SSP_DMACmd(spip->ssp, SSP_DMA_RX, ENABLE);

while (((Channel0_TC == 0) && (Channel0_Err == 0)) || ((Channel1_TC == 0) && (Channel1_Err == 0)));

My SPI is configured for 8bit, so I setup the DMA Transferwidth to the same.

This is inside my SPI send function, so 'n' will be the amount of bytes to be transferred.

The Channel0_TC and Channel1_TC are set correctly to 1 in the DMA interrupt.

But the rxbuf configured for the RX DMA stays empty...

Anyone a pointer what might go wrong here?

Cheers,

Gerard

dma_txconfig.SrcConn = 0;

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,453件の閲覧回数
gvandenbosch
Contributor I

I just found out I made a stupid mistake.

It was solved by removing the & in front of my buffers.

The following changes results in a working DMA on ssp:

dma_txconfig.SrcMemAddr = (uint32_t)txbuf;

dma_rxconfig.DstMemAddr = (uint32_t)rxbuf;

0 件の賞賛
返信