Where to migrate from LPC2387 if 96 kByte RAM turns insufficent

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where to migrate from LPC2387 if 96 kByte RAM turns insufficent

1,406 次查看
bertram_weinzer
Contributor I

We (my company) are using LPC2387. Everything is fine but we're running out of memory. In detail: RAM. We would need more RAM memory by factor 5 we guess. Which processor out of the current NXP range could be a solution for our needs having in mind of keeping necessary code changes in the SW project as low as possible.

标签 (1)
0 项奖励
回复
1 回复

1,292 次查看
b36401
NXP Employee
NXP Employee

Please look at LPC54000 series:
https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-corte...

It has up to 360KB SRAM.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复